IT administrators are the consummate multi-taskers! Never have I seen a job with more to do, more interruptions, and more #1 priorities. KVM-over-IP and Access Systems can be a huge benefit giving IT admins instant, remote access to hundreds or even thousands of servers and devices.
The recent Dominion KX II release (version 2.3) provides a variety of productivity advancements to boost the productivity of the busiest IT admin including: dual/multi-monitor support, launch in full screen mode, HD video resolution, DVI-I support and speedy single mouse mode.
These days there is too much work to fit on a single screen! So the use of dual and multiple monitors is essential. With the new dual monitor feature, the Dominion KX II KVM-over-IP Clients will launch on multiple monitors. Users can control which monitor the Client is launched on and whether the Client is launched in full screen mode.
So, for example, a user can have Command Center in their primary monitor and launch KVM sessions in full screen mode on a second monitor. Full screen mode now features a hidden toolbar for convenient access to all KVM Client functions. Full screen mode is just like a direct connection to a server. Except that you are at your desk, in a meeting or even at home.
For more information on the Dominion KX II’s latest advancements in productivity, security and tiering/cascading, see: