Categories
Keywords
AFCOM Carbon Cap centralized management Data Center Data Center Efficiency Data Center Energy Management Data Center Power Data Center Power Efficiency Data Center Rebate Energy Efficiency Energy Management KVM KVM over IP Power IQ Power Management Power Usage Effectiveness PUE Rack PDU Remote Access VirtualizationSubscribe
Connect on LinkedIn
Category Archives: KVM
Non-Blocked IP Access at Last !
A new Dominion KX II model is now available – the Dominion KX2-808. The DKX2-808 enables 8 simultaneous remote/IP connections to 8 servers or PC’s. The DKX2-808 is unique among the KX II models since it provides “non-blocked” access, i.e. … Continue reading
Posted in Access and Management, Blade Management, Government Security Compliance, KVM
Tagged blade, KVM, KVM over IP, kx, kx2, non-blocked, paragon
Leave a comment
Gartner Data Center Conference
Gartner Data Center Conference Caesars Palace, Las Vegas, NV Monday, December 5-7, 2011 Booth # 42 Come to our booth to see Raritan’s Data Center Infrastructure Management (DCIM) solution – dcTrack. dcTrack brings an even stronger asset, capacity and change … Continue reading
Announcing Dominion LX – Affordable KVM-over-IP for SMB’s
Raritan has just announced the Dominion LX series of KVM-over-IP appliances. The Dominion LX is a family of affordable, high-quality KVM-over-IP switches with single power, single LAN and virtual media. Targeted towards small and midsize businesses (SMB) with less than … Continue reading
Posted in Access and Management, Data Center, KVM, Remote Office Management
Tagged bios, KVM, KVM over IP, Remote Access, Security, smb, virtual media
Leave a comment
KVM Security Article in Inside Networks
In the October issue of the UK’s Inside Networks magazine, on pages 40 to 43, I discuss remote access for IT Administrators with a focus on the security requirements for secure remote access. Click here to access the article (pages … Continue reading
Posted in Access and Management, Data Center, Government Security Compliance, KVM
Tagged KVM, KVM over IP, Security
Leave a comment
When Considering a Centralized Management Solution, Know the Advantages of a Turn-Key Appliance
. . . compared to a more complex hub & spoke approach, which can require significant management overhead of multiple 3rd party servers, constant dB synchronization and complex licensing, appliances enlist a straightforward failover and expansion approach. Licensing is straightforward when compared to the often confusing array of licensing options needed to cover a variety of hub/spoke combinations. As a result, a typical appliance-based solution costs thousands less than a hub & spoke deployment. Continue reading
Dominion KX II Release 2.4 Available
Dominion® KX II is Raritan’s enterprise-class, KVM-over-IP switch that provides anytime, anywhere remote access and control. Release 2.4 provides many new and exciting features including (1) mobile KVM access via Apple iPad /iPhone and (2) digital audio over IP for … Continue reading
For Existing CC-SG Customers It’s Easy to Migrate to a Virtual CC
My last few blog posts have focused on the benefits of deploying the CommandCenter Secure Gateway as a virtual appliance (VA). Now, with the release of CC-SG 5.1, it’s time to talk about how CC-SG hardware appliance users are shifting … Continue reading
Posted in Access and Management, Uncategorized, Virtualization
Tagged centralized management, Virtualization
Leave a comment
Dominion KSX II Firmware Update – Release 2.3
The Dominion KSX II combo KVM/IP and secure console server has been upgraded to include all KX II Release 2.3 features, except tiering/cascading. This includes FIPS 140-2 encryption, Smart Card/CAC and other security features, making it ideal for government, military … Continue reading
Bandwidth Usage for KX II HD 1080p Resolution?
A customer recently asked how much bandwidth the Dominion KX II KVM-over-IP access uses, specifically for the full HD (1920×1080) resolution. This is a common user question. The answer is as follows. There is no fixed bandwidth for the KX … Continue reading
When Deploying a Centralized IT Management Solution, Leverage the Advantages of a Virtual Appliance
Vendors in the IT and data center space are beginning to make their centralized management systems available as a virtual appliance, enabling them to run on leading virtualization platforms. This is the case with Raritan’s CommandCenter Secure Gateway (CC-SG). A new version will be released in November that can be deployed as a VMware virtual machine. Continue reading
Posted in Uncategorized, Virtualization
Tagged data center management, IT management, KVM, virtual appliance
2 Comments