Category Archives: Access and Management

Non-Blocked IP Access at Last !

A new Dominion KX II model is now available – the Dominion KX2-808.   The DKX2-808 enables 8 simultaneous remote/IP connections to 8 servers or PC’s.  The DKX2-808 is unique among the KX II models since it provides “non-blocked” access, i.e. … Continue reading

Posted in Access and Management, Blade Management, Government Security Compliance, KVM | Tagged , , , , , , | Leave a comment

Announcing Dominion LX – Affordable KVM-over-IP for SMB’s

Raritan has just announced the Dominion LX series of KVM-over-IP appliances. The Dominion LX is a family of affordable, high-quality KVM-over-IP switches with single power, single LAN and virtual media. Targeted towards small and midsize businesses (SMB) with less than … Continue reading

Posted in Access and Management, Data Center, KVM, Remote Office Management | Tagged , , , , , , | Leave a comment

KVM Security Article in Inside Networks

In the October issue of the UK’s Inside Networks magazine, on pages 40 to 43, I discuss remote access for IT Administrators with a focus on the security requirements for secure remote access. Click here to access the article (pages … Continue reading

Posted in Access and Management, Data Center, Government Security Compliance, KVM | Tagged , , | Leave a comment

When Considering a Centralized Management Solution, Know the Advantages of a Turn-Key Appliance

. . . compared to a more complex hub & spoke approach, which can require significant management overhead of multiple 3rd party servers, constant dB synchronization and complex licensing, appliances enlist a straightforward failover and expansion approach. Licensing is straightforward when compared to the often confusing array of licensing options needed to cover a variety of hub/spoke combinations. As a result, a typical appliance-based solution costs thousands less than a hub & spoke deployment. Continue reading

Posted in Access and Management, Data Center | Tagged , , | Leave a comment

Dominion KX II Release 2.4 Available

 Dominion® KX II is Raritan’s enterprise-class, KVM-over-IP switch that provides anytime, anywhere  remote access and control.  Release 2.4 provides many new and exciting features including (1) mobile KVM access via Apple iPad /iPhone and (2) digital audio over IP for … Continue reading

Posted in Access and Management, Data Center, Government Security Compliance, KVM, Remote Office Management | Tagged , , , , , , , , | 8 Comments

For Existing CC-SG Customers It’s Easy to Migrate to a Virtual CC

My last few blog posts have focused on the benefits of deploying the CommandCenter Secure Gateway as a virtual appliance (VA). Now, with the release of CC-SG 5.1, it’s time to talk about how CC-SG hardware appliance users are shifting … Continue reading

Posted in Access and Management, Uncategorized, Virtualization | Tagged , | Leave a comment

Dominion KSX II Firmware Update – Release 2.3

The Dominion KSX II combo KVM/IP and secure console server has been upgraded to include all KX II Release 2.3 features, except tiering/cascading.  This includes FIPS 140-2 encryption, Smart Card/CAC and other security features, making it ideal for government, military … Continue reading

Posted in Access and Management, Blade Management, Government Security Compliance, KVM, Remote Office Management | Tagged , , | Leave a comment

Bandwidth Usage for KX II HD 1080p Resolution?

A customer recently asked how much bandwidth the Dominion KX II KVM-over-IP access uses, specifically for the full HD (1920×1080) resolution.  This is a common user question.  The answer is as follows. There is no fixed bandwidth for the KX … Continue reading

Posted in Access and Management, KVM, Remote Office Management | Tagged | Leave a comment

Data Center Disaster Recovery Tools

There are many types of “disasters” that can occur in a data center.  These can range from an all encompassing failure to the loss of certain critical IT services.  These can happen at any time related to human error, system … Continue reading

Posted in Access and Management, Data Center Technologies, KVM | Tagged , , , , | Leave a comment

What to Look for in a Smart Card-Enabled KVM Solution

Using a smart card to access a PC or server that’s within arm’s reach is easy. However, a major challenge is to support this directive in the data center or any application in which users must access multiple servers or PCs that are often located in a separate room, let alone several feet away. Continue reading

Posted in Access and Management, Data Center, Data Center Technologies, Government Security Compliance | Tagged , , , , | Leave a comment